Part Number: TPS7A85 Hello,
Do we have answer for the below problem statement? we wanted to consider the same part our design.
"Once I made the change, the TPS7A85 output appeared unstable and was always lower than 2.5V. Prior to the change, it…
Part Number: TPS7A85 Hi TI Folks,
My case uses TPS7A8500ARGRR, please help to check the schematic design. (The voltage and current are written in the design note)
Especially Vdrop and thermal evaluation.(V n VS Vout)
On the other hand, May I ask VBIAS…
Part Number: TPS7A85
The above design as per webench tool doesn't connect from SNS to ANY-OUT pins for 0.925V output.
Is it issue with the tool , please comment on this.
Part Number: TPS7A85 As per the datasheet, The TPS7A85 can either use external resistors or the internally-matched ANY-OUT feedback resistor network to set the output voltage.
I want to use ANY-OUT pins to set the output voltage, for the following case…
Part Number: TPS7A85 Other Parts Discussed in Thread: , TPS7A83A , TIDA-01232 Hi all, I need some advice. I have to use the TPS7A85 component to meet the following parameters: Input Voltage: 3.5V Output Voltage: 1V Output Current: 2A Allowable Ripple : 1mV …
Part Number: TPS7A85
Hi,
I am looking at a TPS7A85 which is supposed to deliver up to 4A output. I see a die that is marked with 8300 which from my understanding only delivers 2A of output.
Is this normal? I was told TI uses the same die and tweeks…
Part Number: TPS7A85 Other Parts Discussed in Thread: TPS74401 , LP38798 , TPS7B4254-Q1 , TPS709-Q1 Hello,
May I have some questions regarding RCP scheme of LDO devices? In 8.1.19 in TPS7A85 datasheet, it suggests to add a schottky diode to prevent the reverse…
Other Parts Discussed in Thread: TPS7A85 Hi Team,
We have some queries and requirement for LDO. Please check mentioned below queries and Requirement:-
Requirement 1 for LDO(L2):-
Input Voltage:- 3.3V
Output Voltage:- 1.8V
Output Current:- 170mA
Allowable…