Part Number: TPS7A88-Q1 I am trying to simulate the TPS7A88-Q1 IC using LTspice tool. I downloaded the https://www.ti.com/lit/zip/sbvm554
I am getting errors due to some reason
Any ideas what the problem might be?
Here is the SPICE error log:
Questionable…
Part Number: TPS7A88-Q1 With the attached circuit:
VIN = 5.2V
Vout = 0.92 V
Cout = 30 uF
We are seeing about 50 mV of overshoot during startup. Simulation in SPICE shows no overshoot. Please help us find the cause.
Plot of output at startup:
Part Number: TPS7A88-Q1 Hello,
How can I find the stability region for my TPS7A88-Q1 design, for example the minimum required ESR of the ouput capacitance?
Thanks,
Robert
Part Number: TPS7A88-Q1 I'm using the tps7a8801qrtjrq1. If I'm not using one of the channels, how should I connect:
IN, EN, SS_CTRL, NR/SS, OUT, FB, PG
Thanks
Part Number: TPS7A88-Q1 Other Parts Discussed in Thread: TPS7A88 , Hello LDO Team,
Could you urgently let me the information below? Thank you for your urgent help.
1. Does the thermal pad of ACTUAL package has PIN 1 indicator?
2. If yes, could you please…
Part Number: TPS7A88-Q1 Hello I'm using the TPS7A8801RTJR on a PCB, since this part isn't currently available in the distributers stock I may use the TPS7A88QRTJRQ1. I observed in the Datasheet of the TPS7A88-Q1 that the Component has additional Pads…
Part Number: TPS7A88-Q1 Other Parts Discussed in Thread: TPS7A88 Hi there,
As already asked by Lindsey Fike : On page 37 of the datasheet it shows 4 additional pads at the corner of the device marked A1 to A4. I could not find in the datasheet anything…
Hi Gunter,
If you intend to have a safety system, LDO recommended for 1.2 V is TPS7A88-Q1 which will meet the power requirements. For non-safety application, LDO recommended for 1.2 V is TPS74801-Q1.
Thanks,
Susmitha.
Part Number: TMS320F28379D Other Parts Discussed in Thread: TPS7A88-Q1 , SN74LVC8T245 , THVD1452 , TPD4E001 , C2000WARE Hi,
We are planning a custom board for BLDC motor drive application.
1. Can we use TPS7A88-Q1 to power TMS320F28379D? Is there any reference…
Part Number: TPS7A88-Q1 Team,
I am working with the TPS7A88-q1. I was wondering if you could help me get some information on the foldback current limit profile. Is there some kind of equation or method that we could use to estimate the output current…