Hi Hannah,
Thanks for the reply. Please see my response embedded below.
1) We recommend adding a resistor of 10uF to the input.
[VD] We do have a 10 uF to the input. Not attached with the above pictures.
2) Make sure that during layout the IN and OUT…
Part Number: TPS7A92 Hello:
We're using your part TPS7A9201DSKR in our output current 1.2A application.
In our design CFF capacitor CC0201KRX7R8BB103 is assembled, and we have found few failure/shortcircuit cases.
We use several this type capacitor…
Part Number: TPS7A92 Hi,
I'm planning to use TPS7A92 for my project,
this is my requirement,
Vin=5V
Vout = 3.8V
Iout = 1.6A
Ta= 70C
based on datasheet, i have done some calculations,
part has RθJA = 56.9 °C/W, if we calculate the Pd(max) of this…
Part Number: TPS7A92 Hi,
The NR/SS capacitance of TPS7A92 does not have a minimum value in the datasheet. What is the maximum power-on slope of the chip for vout?
Thanks!
Best Regards,
Zixiao
Part Number: TPS7A92 Other Parts Discussed in Thread: TPS7A94 , TPS7A96 , TPS7A53 Hi,
We are using TPS7A92 in our project.
But during bringup of the board, we came to know we need higher current for the IC which is powered by TPS7A92.
So, please share…
Part Number: TPS7A92 Hi Team,
Greetings for the day.
We are using the TPS7A9201 LDO in our Layout Board file. I had attached the images of the Board file and Schematics. Please review the layout and share your feedback with us.
The PCB we are using is of…
Part Number: TPS7A92 Hi Team,
Greetings for the day.
We are using the TPS7A9201 LDO in our Layout Board file. I had attached the images of the Board file and Schematics. Please review the layout and share your feedback with us.
The PCB we are using is of…
Part Number: TPS7A92 Hi Team,
We are using the TPS7A9201 LDO in our Layout Board file. I had attached the images of the Board file and Schematics. Please review the layout and share your feedback with us.
The PCB we are using is of 12 Layers:
IC - Place…