Part Number: TPS7B4250-Q1 Other Parts Discussed in Thread: TL431 , Hi Team,
Could you please help to check if we have an LDO which don' have tracking function which is similar with TPS7B4250-Q1 could support reverse current, reverse voltage and short to…
Part Number: TPS7B4250-Q1 Hi team,
One question about the voltage rating selection of output capacitor.
Considering the short to battery case would happen and battery voltage range is about 9V~16V, so what is your recommendation for the voltage rating…
Part Number: TPS7B4250-Q1 I wonder is there any problem on TPS7B4250 pspice model.
Since I have been not able to see dropout voltage point of this product.
Could you please help me?
From datasheet of TPS7B4250, the definition of Vdrop is
Vdrop = Vi …
Part Number: TPS7B4250-Q1 Hi team,
Is output current clamped to "Output current limitation IOUT(LIM) " if short circuit condition? In this case, does I OUT(LIM) continue to flow until its thermal shutdown?
Regards, Ochi
Part Number: TPS7B4250-Q1 Other Parts Discussed in Thread: TPS7B4254-Q1 , TPS7B4253-Q1 , Hi,
I have looked for this device part number on several vendor sites (Digi-key, Mouser, Newark), and unfortunately have seen that this part is out of stock with an…
Part Number: TPS7B4250-Q1 Hello Team, I have a question. Can TPS7B4250-Q1 use as usual LDO? It means ADJ/EN-pin is able to use as feebback-pin of usual LDO. (Of course, The external voltage divider is required.) I looked at the datasheet it seems reference…
Part Number: TPS7B4250-Q1 Figure 11 of the data sheet seems to indicate PSRR performance of > 90 dB out past 1 MHz, see below.
This seems extremely optimistic. Is this really true?
-Steve
Part Number: TPS7B4250-Q1 I want to get output current more than 50 mA from the device.
Provided, 7 V IN ,5 V OUT and 150 mA output current
In above case, the power dissipation in the device is 300 mW only, less than 350 mW (7 V * 50 mA)
Am I wrong?
…
Part Number: TPS7B4250-Q1 Hi team,
Could you explain the behavior of VOUT when dead short to GND?
Output short circuit protection is described in the datasheet as protected by the current limit and thermal shutdown,
1. Hit current limit (500mA maximum…