Hi
Regarding shorted to another supply, what happen to Vref pin when the Vout is shorted to another supply which is higher than setting voltage and VIN?
I understand that this device has the output short proof to GND and supply. I would like to know the…
Other Parts Discussed in Thread: TPS7B4250-Q1 I would like to confirm the failure mode of TPS7B4250-Q1.
Are there is the possibility below situation by the failure?
- Output pin has some output though ADJ/EN is "Low".
If there is the possibility…
Dear Yamauchi-san,
I thought TPS7B4250-Q1 was working in normal status (Iout<=50mA), but not in short to GND condition(Iout>>50mA). As I said, the current though TPS7B4250-Q1 is so large when VOUT is short to GND, and different devices have different maximum…
Carson-san,
Could you confirm which parameters may be exceed the datasheet spec if customer connect TPS7B4250-Q1(50mA tracking LDO) to BSTOUT and consume 100mA totally(MICBIAS+TPS7B4250)?
Best Regards,
Other Parts Discussed in Thread: TPS7B4250-Q1 I would like to confirm the dropout voltage of TPS7B4250-Q1. I have got the question of it from the customer.
The conditions are; 1. Vin = 5.8V, Io = 40mA 2. Vin = 5.8V, Io = 30mA
Could you please estimate the…
Other Parts Discussed in Thread: TPS7B4250-Q1 I would like to confirm the measures to pin to pin short for TPS7B4250-Q1. The customer is afraid the voltage supply and GND are shorted by the short 2pin and 3pin.
1. In the case that we add the resister between…
Other Parts Discussed in Thread: TLV704 , LP2985-N , TPS709 , LP2992 , TPS7A25 hi Team,
trying to find TI compatible parts with
S-1200B35-M5T1U /SOT-23-5
is the following part a good fit?
LP2985-N
S-1212B28-M5T1U /SOT-23-5
closest i found is the
TPS7B4250…
Hi Charlie,
My apologies, I was intending to refer to the TPS7B425x-Q1 family (TPS7B4254-Q1, TPS7B4253-Q1, TPS7B4250-Q1). I am not sure what happened to my "42." These devices have an operating input voltage range up to 40 V.
Very Respectfully…
Part Number: TPS7B67-Q1 Other Parts Discussed in Thread: TPS7B4250-Q1 , TPS1H100-Q1 Dear, Sir.
My customer is considering to apply TPS7B6750-Q1 for their system.
Sounds like, OEM is requiring AEC-Q100-012 short circuit reliability on IC's.
Sorry to…