Part Number: TPS7B4261-Q1 Tool/software: Hi Team,
when the device output is short, PG gets low. However, after the short condition has gone, still PG is low.
What kind of condition, PG get recover to High? such as ADJ off to on
Best,
Shoo
Unfortunately, we do not have a tracking LDO (the ones which target an external voltage) that could fit within your requirements
The closest I could find was TPS7B4261-Q1 Automotive, 300mA, 40V, Voltage Tracking LDO With PG datasheet but it has no current…
What is the difference between a tracking LDO and a regular LDO?
A regular LDO reacts to changes in the input voltage, V IN and the load current, I OUT by dynamically minimizing error between the feedback voltage, V FB and an internal reference voltage…