Part Number: TPS82130 Hello,
What's the package height tolerance of TPS82130? The data sheet describes only the Max value, but what about the Min one?
Best regards, Shinichi Yokota
Part Number: TPS82130 Hi Team,
Could TPS82130 supports >6VOUT? If I intentionally set FB so that VOUT_SET is higher than 6V, what would happen? What influences maximum VOUT to be just 6V if minimum toff is allowed to do this?
-A
Part Number: TPS82130 Hi.
I use the TPS82130 with a 5V output. What happens to the device when an external voltage of more than the output voltage (ex. 5.5V) is applied to Vout? Will the device be damaged?
Part Number: TPS82130 Hi team,
My customer consulted me the following two questions about TPS82130. Could you pls help me to answer him.
Questions:
Whether the threshold of high-level input voltage and low-level input voltage of EN pin can be…
Part Number: TPS82130 Dear support team,
I am trying to use the TPS82130 to generate a low noise, 6V output with the following circuit, however, the circuit keeps failing.
I have tried 3 PCBs,
The first one gives a strange ~4.8V output, sometimes…
Part Number: TPS82150 Other Parts Discussed in Thread: TPS82130 , TPS82140 , Hi team
Could you help check if TPS82130/TPS82140 are the drop-in replacement option for TPS82150?
My customer met the shortage of TPS82150 and wants the backup solution…
Part Number: TPS82130 Hi,
I created the circuit using the TPS82130 device. The input voltage of this circuit is + 5V and the output voltage is -5V. I would like to ask you about the startup behavior of this device. At startup, about + 0.5V is output…
Part Number: TPS82130 Good Morning,
regarding the labeling "LBL:" information, I've know that this is the identifier for the original STC packing sequence of the batch but to clarify the LBL must match on all labeling regarding to the reel?
This is…
Part Number: TPS82130 Hello E2E Experts,
Good day.
Based on the application note, Resistance Junction to Board (in section 4, Page 10) is a more representative value for conduction-to-board cooled components than Resistance Junction to Case (Bot)…
Part Number: TPS82130 Other Parts Discussed in Thread: LMZM23600 Hi
customer application: Vin=7V~16V, Vout=6.3V, Iout<0.5A
but in datasheet, the max output is 6V in datasheet.
I want to check with you if Pin7 PG is floating, not used, can output…