Part Number: TPS922052 I have built and have been testing the following circuit based on the TPS922052. I used a draft tool shared with me to compute some of the values, and then looked at the EVAL schematic for further information. I'm putting the chip…
Other Parts Discussed in Thread: TPS922052 , TPS922055 , TPS922054 , TPS922053 How to design the CSP and CSN pin components for TPS922055 / TPS922054 / TPS922053 / TPS922052?
Tool/software: The device goes into sleep mode after 57ms and it takes about 5ms until the full LED current is present.
Question is how to prevent sleep mode. Idea is to have a 160ns pulse every 50ms to prevent sleep mode. Not sure what the intend is…
Part Number: TPS922052 Tool/software: Hello guys,
One of my customers is considering using TPS922052 for their new products.
At this moment, they have the following questions. Could you please give me your reply?
Q1. They'd like to control LED brightness…
Part Number: TPS922052 What should I do if I want to operate at 100% output without a processor such as an MCU?
If necessary, please tell me about the circuit and timing of ADIM/HD, EN/PWM, Vcc, etc.
Other Parts Discussed in Thread: TPS922052 , TPS922055 , TPS922054 , TPS922053 Is there a simulation model for TPS922055 / TPS922054 / TPS922053 / TPS922052?
Other Parts Discussed in Thread: TPS922052 , TPS922055 , TPS922054 , TPS922053 Is there a calculation tool to help me design the external components for TPS922055 / TPS922054 / TPS922053 / TPS922052?
Part Number: TPS922052 There is no clear description of the electrical characteristics, so I asked just to be sure.
Is the resolution of analog dimming up to 8 bits? (Is this due to the specifications of the internal DAC?)
For example, even if FADIM…
Part Number: TPS922052 Other Parts Discussed in Thread: TPS92641 ,
Using TPS92205xEVM
Input voltage 48V
Connecting to a single COB LED (18V / 500mA)
PWM frequency (for ADIM + PWM input) 4KHz
I'm initializing Flexible Dimming mode as described…
Part Number: TPS922052 Other Parts Discussed in Thread: TPS92641 , TPS922054 Tool/software:
Hello guys,
One of my customers is considering using TPS922052 to their new products.
At this moment, they have the following questions. Could you please…