Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: TPS92410 Hi,
Good Day. The customer downloads the TPS92410 PSpice Transient Model and generates part in the edit tab.
He made copied and paste all files inside the right folders but doesn't work…
Other Parts Discussed in Thread: TPS92410 , PMP6021 Hello,
I'm looking to use the TPS92410 as a dimmer control. The device specifies that it is capable of analog dimming and states in section 7.1 of the datasheet that it's possible to use a 0-10V input…
Other Parts Discussed in Thread: PMP6021 , TPS92410 , TPS92411 Hello! I tried to do LED driver board based on PMP6021 document. It works, but I have the problem - when I try to use ADIM input (with potentiometer or from external voltage source), I see the…
Other Parts Discussed in Thread: TPS92410EVM-001 , TPS92410 I'm working with the TPS92410EVM-001, and have the ADIM pin/test point connected to a GPIO on my micro. I need to turn on/off the LEDs very fast (30-60-Hz) but have noticed that they are very…
Other Parts Discussed in Thread: TPS92410 , TPS92411 , TPS92561 I'm looking for a simple circuit to drive strings of LEDs that require 160v @ 100ma. The TPS92410 looks ideal but I'm wondering if the TPS92411 drivers could be omitted and just have …
Part Number: TPS92411 Other Parts Discussed in Thread: TPS92410
Deal All
I have apply to TPS92411 for our project. TI_question(TPS92411_PowerPAD).pptx
Please check to my question(Refer to atteched file)
Thanks and BR
PJ
Part Number: TPS92411 Other Parts Discussed in Thread: TPS92513 , TPS92410 , , UCC28700 , LM3447 I currently have a SMPS generating 24V, 2A output, which is running two individual TPS92513 It is working quite well, but the problem is that it takes up quite…
Binod,
Here are some products I think are similar that could work for you. I'll email the product lines who own these parts internally with a link to this thread so they can provide further comments.
UCC28C43-EP
TPS92410
TPS92660
LM3401
TPS92630…
The TPS92410 version has many performance advantages over the discrete circuit:
1) A dimmer detect circuit senses when a leading edge dimmer is present and switches the current reference to DC providing more consistent holding current for a triac dimmer…
Other Parts Discussed in Thread: TPS92210 , LM3447 , TPS92075 , TPS92410 Is it possible to modify the EVM-647 to drive fewer leds at 350mA, looking for a load of 3-6 watts. Are there other fly back transformers already design for these different application…