Hello Hailee,
Currently, we are checking the feasibility using simulation and we don't have the real board for the TPS92610-Q1 IC test.
Could you please reconfirm the above mentioned issue from you end and reconfirm (Default, Fault pin as floating…
Part Number: TPS92610-Q1 Hi,
In which conditions is reported the Junction to ambient thermal resistance?
Your ref document does not explain nothing about the HTTSOP package.
According to our specifications, this component is just a little bit too tight…
Part Number: TPS92610-Q1 Hello Team,
I'd like to make sure about the behavior of TPS92610-Q1.
In datasheet, this device detect fault condition during PWM pin is high and it will be ignored when PWM pin is low. At customer test, they observed that…
Part Number: TPS92610-Q1 hello,
i have one question about the TPS92610-Q1 signal LED short detection, if i do not need signal LED short detection,
i checked the DATASHEET, i think i should tie the SSH ,SSL together ,like the following pciture.
but i would…
Part Number: TPS92610-Q1 Other Parts Discussed in Thread: TPS92633-Q1 , TPS92633 Team,
Do you have detail on the calculation required to seize the pull up of on the fault pin of 'n' number of TPS92610-Q1 attached together to create a "one-fails–all-fail…
Part Number: TPS92610-Q1
Hi Team,
As part of our customer's way of improvement and internal inspection, can we request for your recommendation about acceptable void rate on the thermal pad of TPS92610-Q1?
Thanks in advance! Kind Regards, Jejomar
Part Number: TPS92610-Q1 Other Parts Discussed in Thread: TPS92611-Q1 Hi,
Customers will have TPS92610-Q1 / TPS92611-Q1.
* Questions
The design specification is the output current Type 260mA1CH, Type450mA1CH.
For the 260mA specification, it is assumed…
Part Number: TPS92610-Q1 Is it necessary to bias the PWM pin at any level if just using it to turn on the LEDs for a short period (1% duty cycle) using a microcontroller. I need to minimize total current draw in my application.
Part Number: TPS92610-Q1 Hi all,
I have a few questions about diagnostic functionalities of this IC.
Can you tell me why DIAGEN function is implemented in this IC? Is it because the current is not enough when the input voltage is low?
Can you tell me…
Part Number: TPS92610-Q1 What is the max negative input voltage on SUPPLY and EN pins for a TPS92610-Q1? I need transient and reverse voltage protection.