Part Number: TPS92610-Q1 Hello,
I am looking for validation of dropout values of TPS92610 .
In Datasheet, I can see this:
I have download spice model of IC from TI websites, that shows for current of 350mA Dropout approx 0.8V (including sense…
Part Number: TPS92610-Q1 Tool/software: Hi,
I am using TPS92610Q single channel IC for for TAIL LED function. when diagnostic detect single LED short or open, IC generate 2mA retry current which cause LEDs dimming with very low intensity.
How to…
Part Number: TPS92610-Q1 Other Parts Discussed in Thread: TINA-TI Tool/software: Hi Team,
I need a transient macro for TPS92610 / 611 / 613. The Macro model available on Ti's website is corrupted.
Best Regards
Vishal Kakade.
Part Number: TPS92610-Q1 Hi,
In which conditions is reported the Junction to ambient thermal resistance?
Your ref document does not explain nothing about the HTTSOP package.
According to our specifications, this component is just a little bit…
Part Number: TPS92610-Q1 Tool/software: Dear TI team,
I am working on a project that is going to use the TPS92610-Q1, and I need to know the effect produce by the temperature. I mean, I need either to math or simulate the effect that the temperature…
Part Number: TPS92610-Q1 Other Parts Discussed in Thread: TPS92621-Q1 Hello Team,
We are currently using TPS92610-Q1 (Single-Channel Linear LED Driver) in one of our designs.
The operating temperature range is -30°C to 85°C for our design. We…
Part Number: TPS92610-Q1 hello,
i have one question about the TPS92610-Q1 signal LED short detection, if i do not need signal LED short detection,
i checked the DATASHEET, i think i should tie the SSH ,SSL together ,like the following pciture.
but…
Part Number: TPS92610-Q1 Hello Team,
I'd like to make sure about the behavior of TPS92610-Q1.
In datasheet, this device detect fault condition during PWM pin is high and it will be ignored when PWM pin is low. At customer test, they observed that…
Part Number: TPS92610-Q1 Other Parts Discussed in Thread: TPS92633-Q1 , TPS92633 Team,
Do you have detail on the calculation required to seize the pull up of on the fault pin of 'n' number of TPS92610-Q1 attached together to create a "one-fails–all…
Part Number: TPS92610-Q1 Other Parts Discussed in Thread: TPS92611-Q1 Hi,
Customers will have TPS92610-Q1 / TPS92611-Q1.
* Questions
The design specification is the output current Type 260mA1CH, Type450mA1CH.
For the 260mA specification, it is…