Part Number: TPS92611-Q1 hi expert
i saw the following data in our datasheet.
Q1: if i use 6.8KΩ to pull up to 3.3V voltage supply.(it means external pullup current is 3.3V/6.8KΩ=485uA). what the range of Vol(fault)?
Q2: could you share the…
Part Number: TPS92611-Q1 Hi team,
Customer need a to build a PWM high side switch in theiir system powering off the 5V supply. When the output short to ground, the current increase will pull low the 5V supply so is not expected. Therefore they are thinking…
Part Number: TPS92611-Q1 Other Parts Discussed in Thread: SN74AHC1G09-Q1 , The absolute maximum rating for the PWM input is -0.3 to 45 V. I would assume that there is a reverse bias diode on the inputs, and the limit of -0.3 V is there to stop there being…
Part Number: TPS92611-Q1 Hi team,
Customer is using tps92611-q1 to generate constant current source for High voltage interlock system. As the external load increasing, the current will decrease to 4mA. Could you please help me understand how the device…
Part Number: TPS92611-Q1 Thanks for your support
When the LED Driver TPS92611-Q1 directly enables 100% duty cycle, the chip output current becomes smaller and smaller as the external resistive load slowly increases. How does the current behave when less…
Part Number: TPS92611-Q1 team,
can you please confirm that this ~400ohm low side resistor is not going to affect performance of the TPS92611-Q1 as long as we have enough drop out voltage?
Part Number: TPS92611-Q1 Hi,
Do you have any idea how to reduce TTSD (from datasheet=173°C) value at which the driver turns off.
My wish is for it to turn off at 100°C. Do you have any solution for that?
Many thanks