Part Number: TPS92612-Q1 Hello,
Do we have recommended values for PWM input max input current across temperature/voltage range?
Thanks,
Alberto Gonzalez
Part Number: TPS92612-Q1 Other Parts Discussed in Thread: TPS92621-Q1 Hi, My customer is looking for a p2p alternative to OnSemi's NSV45060JDT4G (Adjustable Constant Current Regulator & LED Driver). The CrossRef tools does not know the OnSemi part…
Part Number: TPS92612-Q1 Other Parts Discussed in Thread: TPS92612 Hello TI Support,
I want to use the TPS92612 in a design. I would like to run it above 20Khz but lower than 100KHz. Would this be possible to do with the TPS92612.
What are the limitation…
Part Number: TPS92612-Q1 Hello Concern,
We are using TPS92612-Q1 in our Application - as we have a requirement of Short to Battery protection.
But when we are shorting the OUT pin to VBAT --> LED Driver got damaged (After Reset Showing the 0.4V @ OUT…
Part Number: TPS92612-Q1
Hi,
My question is on TPS92612-Q1. Does this LED driver support the below configuration?
Typical Vf (LED)=2.35V and maximum current that I am sourcing 44mA from Out pin of the IC.
Can PWM pin of the IC can be connected directly…
Part Number: TPS92612 Der Sir/Ms.
My customer compares TPS92612 with TPS92612-Q1 data sheet, but can't compare the difference from the characteristic table. The car certification will guarantee the yield rate. I compare the value of MTBF/FIT is the same…
Part Number: TPS92612-Q1
I need to drive my LEDs with a very low duty, typically 0,1%. With a PWM frequency of 1KHz (1000uS period) and a PWM input of 1uS positive, 999uS Gnd, the LEDs flicker, When I look at the signals, I see that LED output sometimes…
Part Number: TPS92612-Q1 Other Parts Discussed in Thread: TPS92612 , TPS92633 This component appears unobtainable. Lead times I see are 73 weeks. Is this going to improve, or do I just need to design in a replacement part? TI seems to be worse than most…