Part Number: TPS92662-Q1 Hi team,
My customer has been evaluating TPS92662-Q1 by using the EVM board, and changed the value of R_SENSE eresistor to maximize the peak current threshold. However, IC temperature gets high when doing it, and the customer…
Part Number: TPS92662-Q1 I have a question about the UART message structure for the tps92662-q1. I'm trying to control an array of LEDs and just realized there isn't tech documentation on the UART message to set the PWM values. Is there a tech doc…
Part Number: TPS92667-Q1 Hi,
we recently get to finalize the prototype of a model of ours of medical lamp by using 6 x TPS92662Q1 each one driving 24 LED (it means 2 LED each switch), and found out or it looks like the TPS goes into some kind of protection…
Part Number: TPS92662-Q1 I connect the led driver to the USB-UART converter and send a UART packet {0x87,0x20,0x80,0xA0,0x48,0xC6} for configuring the SYSCFG register, according to the datasheet, the ACKEN bit is 1, so it can receive the return value…
Part Number: TPS92662-Q1 I connect the led driver to the USB-UART converter and send a UART packet {0x87,0x20,0x80,0xA0,0x48,0xC6} for configuring the SYSCFG register, according to the datasheet, the ACKEN bit is 1, so it can receive the return value…
Part Number: TPS92662A-Q1 TPS92662QPHPRQ1 and TPS92662AQPHPRQ1
what does A mean and present ?
what is the difference between TPS92662QPHPRQ1 and TPS92662AQPHPRQ1?
Part Number: TPS92662-Q1 Other Parts Discussed in Thread: TPS92664-Q1 , Dear Specialists,
The customer is considering TPS92662-Q1 and TPS92664-Q1.
They have a question.
Could you please advise.
They need to obtain the answer as soon as possible.
---
Regarding…