Part Number: TPS929120-Q1 Our computer serial tool connects the TX and RX of TPS929120, configures the baud rate to 115200, and sends data "55 80 61 02 49" after power on. TPS929120 TX has no response output and cannot communicate normally
…
Part Number: TPS929120-Q1 Other Parts Discussed in Thread: TPS929120EVM
Hi,
I have a problem that there is an open circuit when Vin-Vout is very close. Sometimes it even cause communication error. I would like to check first if it is reasonable. …
Part Number: TPS929120-Q1 Other Parts Discussed in Thread: USB2ANY Hello,
I'm trying to get the autoscan mode to work, but I'm not shure what I am missing. I want to get the MAXOUT for calculation of the ideal drop to set the output voltage for the…
Part Number: TPS929120-Q1 Hi there,
I see this from TPS929120-Q1 datasheet ,but I cannot figure out why.
"however TPS929120A version has EEP_DEVADDR[3] bit set to 1 as default. It allows up to 16 pieces of TPS929120-Q1 on same FlexWire bus accessible…
Part Number: TPS929120-Q1 Hi Team,
Could you possible help to clarify what does it mean by" Initialization timer setting EEPROM register" of 0xCAh register of TPS929120-Q1?
And if customer could read or write TPS929120-Q1 register under the condition…
Part Number: TPS929120-Q1 Other Parts Discussed in Thread: TPS929121-Q1 ,
For the 12-channel automotive high-side LED drivers used in automotive lighting, there are a couple of parts available, including TPS929120QPWPRQ1, TPS929120AQPWPRQ1, TPS929121QPWPRQ1…
Part Number: TPS929120-Q1 Hi
If we set the output current 75mA, is it correct the current accuracy is +/-5%?
And the worse case the output current may go up to 75mA x (1+5%) = 78.75mA ?
Part Number: TPS929120-Q1 Dear team,
Customer want to confirm if one CAN transceiver could work with 2 TPS929120 like figure 149 shows.
Thanks.
Best regards,
Sammi