Part Number: TPSM265R1EVM Setting up the evm for 12V ouput. with a 1.2k reistor for the load to draw 10mA. Works well with input voltages up to 50V but anything higher and the evm blows up. I'm putting 58V but he evm should be able to handle up to 65V…
Thank you for the quick reply.
I just received the TPSM265R1EVM evaluation board and checked its operation at Vin = 5.4V, Iout = 100mA. The output appears to be stable at an input voltage of 5.4V. I do, however, see the output start to drop as I decrease…
Hi Theo,
Thanks for the update, let us know if you have any further questions. Alternatively, you may also use our evaluation module as a comparative measurement
https://www.ti.com/tool/TPSM265R1EVM
Thank you
-Arief