Part Number: TPSM53604 I have several TPSM53604 devices on a board. All of them are working properly except for one which is set to create a 2.5V output. My schematic looks the same as the one generated by webbench. The feedback resistors are 10K and…
Part Number: TPSM53604 Other Parts Discussed in Thread: LMZM33604 I have a design where this device supplies 5V to my PCBA. My PCBA has a low current draw sections and a high current draw section. When I push a button, a P-FET is used to allow power to…
Part Number: TPSM53604 Hi everybody,
On my board, I will use several TPSM53604 for different voltage supply.
Do you think, I have to use the EMI filter for each supply ?
Regards,
Charles
Part Number: TPSM53604 Hi,
I will plan to use TPSM53604 for negative output. Refer to the document as below. I am no idea about the value of Cbulk. Would you help to suggest the better value of Cbulk?
www.ti.com/.../snva897
Thanks,
CC
Part Number: TPSM53604 Hi, I hope you are doing well right now. Our customer requested for the bxl file of TPSM53604RDAR however it is not available on our website. I would appreciate if you can share with us the bxl file for this part number. Thank you…
Part Number: TPSM53604 Other Parts Discussed in Thread: LMZM33606 , TPSM82813 , LMZ14201 Hi I am looking for aerospace and defense grade part like TPSM53604/3/2 but current ratting should be more than 6A. Please suggest if you have any part.
Part Number: TPSM53604 Hi, Could you tell me about Pin13? Pin13 names are different for Datasheet and ”EVM and Webench". Which is correct? And Are the functions different between V5V and Vcc? Regards, Yusuke
Part Number: TPSM53604 Tool/software: WEBENCH® Design Tools Webench tool recommends a capacitor is added to the "VCC" pin which I assume is the V5V pin referenced in the datasheet, however, there is no mention of needing any form of bypass capacitor or…
Part Number: TPSM53604 Team,
can you advise what is the spec. for Maximum Duty Cycle DMAX and Minimum ON Time tON MIN for the TPSM53604 module?
Couldn't find this in the datasheet.
Thanks for your help!
Part Number: TPSM53602 Other Parts Discussed in Thread: TPSM53604 , TPSM33625 , TLVM23625 Hi,
I'm planning on using TPSM53602RDAR. The datasheet clearly states requirements for both input and output capacitance, output capacitance as a function of…