Part Number: TPSM63602
This part can output 1V to 16V with an input of 3V to 36V. However, it's called a Step-Down device.
Does this mean, for a 16V output, I must use an input voltage greater than 16V?
Or can I get a 16V output from 12V input?…
Part Number: TPSM63602 HI teams,
I have one question regarding the circuit for generating negative voltage with TPSM63602RDHR. In datasheet, VLDOIN is connected to the VOUT pin (GND), but in the PSpice model, it is connected to the GND pin (VOUT), Which…
Part Number: TPSM63602 Other Parts Discussed in Thread: LMZ34202 I am considering using the TPSM63602 buck converter in a system to generate 16V output based on a 36V input voltage. The TPSM6302 is rated for an input voltage range of 3V to 36V so my application…
Part Number: TPSM63602 Hi TI engineers,
I encountered an issue while testing the TPSM63602V3. I observed that one half of the IC exhibits a notable temperature increase, even under no-load conditions. I've attached the schematic, thermal distribution…
Part Number: TPSM63602 Hello,
We designed a Power Supply circuit using the Webench Designer for our application where our circuit will be powered by a LIFEP04 4S Battery Pack and we need to step down the voltage to 5V DC. We chose TPSM63602V5 for it…
Part Number: TPSM63602 Other Parts Discussed in Thread: TPSM63603EVM For the chip TPSM63602,
1. the data sheet give a recommended layout, but that does not connect the VOUT pins to the FB and VLDOIN pins,
I want to know what is the recommended approach…
Part Number: TPSM63602 Hi team,
On the datasheet 8.3.10 it states that VCC should be connected to AGND as below.
However, on Fig. 9-1, the VCC is connected to PGND as shown below.
Should VCC be connected to the AGND or PGND?
Best Regards…
Part Number: TPSM33615 Other Parts Discussed in Thread: TPSM63602 Tool/software: Hello team,
Can TPSM33615 be used at the below condition? According to the datasheet, Vout (TPSM33615 can output) is up to 14V.
Vin: 18V~30V (24V typ) -> Vout: 15V, 1A…
Part Number: LMR14020 Other Parts Discussed in Thread: TPSM63602 Tool/software: Hi TI Team,
I need an inverting voltage regulator with the following specifications:
Input voltage: 5V
Output voltage: -5V
Output current: 1A to 1.5A …
Part Number: TPSM63606 Other Parts Discussed in Thread: TPSM63602TPSM63602, Whether it can be used produce -15vdc from a 12 v input. If possible, where can I find design tool for -ve output. and example schematic.
The Webench design tool is not allowing…