Part Number: TPSM82866C Other Parts Discussed in Thread: TPS544C26 , TPS542A50 , LMR36503 , TPSM365R3 Tool/software: Hello, in the TI product, I'm finding a programmable voltage regulator IC with an adjustable voltage of 0–5V for I2C, SPI, or UART interface…
Part Number: TPS62827 Other Parts Discussed in Thread: TPS62868 , TPSM82866C Tool/software: Hi,
We want set 2 output voltage level 2.1V and 2.5V. We using N-MOS in parallel the resistor on FB pin, is it may have any side effect? thanks!
Part Number: TPS62871 Other Parts Discussed in Thread: TPSM8287A12 , TPSM82866C Tool/software: Hi Sir :
Regarding TPS62871, I have the following questions to ask. Also, please help check the schematic diagram in the attachment. The selected chip is…
Part Number: TPS62870 Other Parts Discussed in Thread: TPS62869 , TPSM82866C Tool/software: Hi,
We may using TPS62870 to using on Vout 1.2V and 1.8V condition.
How to optimization comp value in these two voltage?
I use wenbench tool but seem Rcomp…
Part Number: TPSM82866A Other Parts Discussed in Thread: TPSM82823A , , TPSM8287A06 , TPSM82866C Tool/software: Hi, could you clarify how the VOS pin should be connected and what its function is vs FB? Looking through the datasheets of a few similar part…
Part Number: LM21215A Other Parts Discussed in Thread: TPSM82866A , TPS62870 , TPSM82866C Tool/software: Hello,
My customer was using the LM21215AMHE-1 under the following conditions.
- INPUT : 5V, OUTPUT : 0.9V, LOAD : 6A
They designed the circuit…
Hi Albert,
The TPSM devices are power modules, which integrate the die and an inductor and sometimes some capacitors. So, they are larger than just the TPS6287x IC. All of these devices are designed for your application, with high efficiency and small…