Hi Tahar,
Tahar Allag said: When power is applied, if no external clocking signal is present on the SYNC pin, the device operates at the switching frequency set by the internal or an external timing resistor. It is permissible for the SYNC signal to become…
Part Number: TPSM846C23 We would like to modify the TPSM846C23 output voltage in the field, over-riding the resistor set default by loading a value from non-volatile memory at power-on.
How many times can the non-volatile memory be written? I could not…
Part Number: TPSM846C23 Hello,
This is regarding the TPSM846C23 DC DC CONVERTER (0.35-2V). On page 22 of the datasheet, it provides a table with various RSET / VOUT pairs. However, the options for 0.9V does not agree with the formula.
Shouldn't a value…
Hey Sujith,
We don't have any dedicated programming guides, instead we suggest you read through the datasheet as that will provide all the information you need. You can purchase a parallel operation EVM and work from there. https://www.ti.com/tool…
Part Number: TPSM846C23 Hi Expert,
Do you have more suit solutions compare with below devices? the size is priority concern for customer design, thank you.
VPN
Vin Range(V)
Vout Range(V)
Imax(A)
Size(mm)
LTM4647
4.7~15
0.6~1.8
…
Part Number: TPSM846C23 Other Parts Discussed in Thread: TPSM846C24 , Hi Team,
We are using the power module as for power suppling our FPGA core rail.
The power on and boot sequences control introduced AND Gate and Buffers, I'd like to use internal LDO…
Part Number: TPSM846C23 Other Parts Discussed in Thread: TPS53688 , TPSM846C24 , TPSM8D6C24 , Hi team:
My customer want to replace EM2140 device in their Stratix-10 platform, At the beginning , we are promoting TPS53688, but after understanding of their power…
Part Number: TPSM846C23 Other Parts Discussed in Thread: TPS51200 , TPS53915 , TPS546A24A Hi Experts,
I am trying to help on of our customer with the below concern:
He has a project have to drive DDR3/4 DRAM on board and require PMBUS control He already…
Part Number: TPSM846C23 Other Parts Discussed in Thread: TPSM846C24 , Hi Team,
I am looking for an alternate device for TPSM846C24. if we do not need the PMBUS function, could it be disabled? need to add the external resistor?
Part Number: TPSM846C23 Other Parts Discussed in Thread: TPSM846C24 , SN74LVC2G07 Hi team,
I just want to double check the input interface of EN-pin quickly.
Does EN pin accept 3.3V CMOS input?
Regards,
Itoh