Hi,
Not sure if you have the similar problem as in the below post.
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/844446/tpsm846c23evm-806-why-ic2-needs-certain-delay-in-tpsm846c23evm-806-for-every-data-byte…
Part Number: TPSM846C23EVM-806 Other Parts Discussed in Thread: TPSM846C23 Hi,
I am trying to establish IC2 communication between TPSM846C23EVM-806 and TIVA TM4C1294XL to control the output voltage of the TPSM846C23EVM whose default voltage is 0.6V. I…
Part Number: TPSM846C23EVM-806 Other Parts Discussed in Thread: TPSM846C23 With no load connected I always read 0xE018. The MSB of 0xE0 makes sense but I do not understand why do I read the LSB as 0x18 as you can see from the snapshot below ?
Thanks in advance…
Part Number: TPSM846C23EVM-806 Other Parts Discussed in Thread: TPSM846C23 Hi,
I would like to extend the remote sensing points in TPSM846C23EVM-806 but I am little bit confused. The block diagram below is what I want to test exactly to see it TPSM846C23…
Hi,
bala sund said: when I tried to write first time the data is written to the slave which i could able to capture in I2c analayzer
I think it is a good improvement. Earlier, I thought you said it didn't work at all.
Can you at every place where…
Hi Ben,
According to the datasheet, the timeout counter is supposed to start at the beginning of the START condition. This means that the counter should start to down count when you start the first transaction at line 8.
The application can program the…
Hi Adrian,
There are multiple connections on the parallel EVM to enable the two-phase configuration (SYNC, VSHARE, ISHARE pins, among other modifications), so it would not be easy to modify the parallel EVM for single phase operation. You would likely…