Hi Hirotsugu,
Yes, you are right, my bad. Bode plot cannot be measured with Cff between Vout and Vadj on this module!
Regardless, this module does not seem to be a good fit for your application. I wish I could do better.
Regards,
Yitzhak
Part Number: TPSM84A21 Hi team,
I would like to measure the loop response of TPSM84A21EVM.
There is R7(0 ohm) on the EVM, can I measure changing R7?
Is it possible to measure even if there is 10-ohm between VOUT and VS+ inside?
Best Regards,
Part Number: TPSM84A21 Hello,
I have multiple regulators off a single 12V rail off a server. The switching freq of the 12V input is unknown and can vary from server to server. Are there any recommended input filter values for use with this regulator?
…
Part Number: TPSM84A21 Other Parts Discussed in Thread: TPS54824 Hi Team,
Our customer would like to use TPSM84A21 for Xilinx Zynq Ultra+ MPSoC XCZU7CG-1FFVC1156E. I have shared the link to the recommended voltage regulator IC for FPGA in the link below…
Part Number: TPSM84A21 I am looking for a DC-DC Switcher for running the FPGA Core Power rail. My Requirement is as below
1. Vin - 5 to 14V
2, Vout = 1V
3. Iout = 10A
4. Small Footprint as far as possible with more than 90% Efficiency.
Please suggest…
Part Number: TPSM84A21 Hello,
Is it possible to communicate the value of the shielded inductors integrated in the component (on the output)?
I would like to calculate the cutoff frequency of the filter realised by those inductors associated with the Cout…
Part Number: TPSM84A21 Other Parts Discussed in Thread: TPS54A20 Hi,
As far as I could understand (referring to slva750a) the internal switching mechanism of this part is based upon a N steps looping machine, where only 1 step interval is dedicated to…