The TPSM8A28 is uses a COT control similar to the IR3473 and IR3475 and
operates over the input voltage range of 4 to 6V and has switching
frequency options of 600kHz, 800kHz and 1000kHz.
the TPSM8A28 would be suitable power module for both IR3473…
Part Number: TPSM8A28 Hi team,
My customer found TPSM8A28 efficiency gap from the datasheet.
He would like to check VIN=12V, VOUT=5V, IOUT=4A, 600kHz FCCM frequency of TPSM8A28.
In the datasheet Figure8-9, it looks like ~93%. But the Webench shows…
Part Number: TPSM8A28 Hi team,
My customer concerns about the reflow of TPSM8A28. My customer is likely to place these modules on the first reflow side. So they concerns about the risk which the modules drop off from PCB during the second reflow like…
Part Number: TPSM8A28 Other Parts Discussed in Thread: TPS548A28 , TPS548A28EVM Hi Team,
My customer wants to use TPSM8A28 in their system as 3.3V power input condition. Do you think there are any risks such the use case? I can not check it on Webench…
Part Number: TPSM8A29 Other Parts Discussed in Thread: TPSM8A28 Hi team,
Is the efficiency curve on the TPSM8A28/9 datasheet applicable for both TPSM8A28 and TPSM8A29?
Or, does it have any difference?
The current range looks <15A which is only supported…
Part Number: PTR08060W Other Parts Discussed in Thread: TPSM843620 , TPSM8A28 Tool/software:
I'm trying to use a switching regulator to step 12V DC down to 2V DC, however it is not achieving this at all (even with no load connected), and is outputting…
Part Number: TPS62873 Other Parts Discussed in Thread: TPS62876-Q1 , TPS6287B25 , TPSM5D1806 , TPSM8A29 , TPSM8A28 , TPSM843B22EVM , TPSM843B22 , TPS74701
Hi,
We are planning to use the mentioned part number TPS62873N0QWRXSRQ1 in our design for the…
Part Number: PMP9444 Tool/software: Hello ref design team,
My customer is working on power supply design for Xilinx FPGA. TI reference design PMP9444 is an approved solution for Xilinx UltraScale Kintex part.
there are 2 questions:
I am not…
Hi Grady
You can also look into
TPSM8S6C24/TPSM8S6B24 stackable
TPSM843A26/TPSM843B22 non stackable
TPSM8A28/TPSM8A29 non stackable
Are you looking for two 13A rails or single 26A rail?
Thank you
Savith