Hello support!
Do you have some tools for calculating pcb anthenna for this device?. I tried to find something but I saw just Antenna Design Guide for the TRF79xxA (Rev. C) that is all...
BR, Oleg
Part Number: TRF7964A Hello!
We have confirmed the RSSI of TI TRF7964ARHBT.
When RSSI was measured, it was 7 at the main receiver, confirming that it was the maximum RSSI.
However, in the specification (TRF7964A SLOS787J –MAY 2012–REVISED MARCH…
Part Number: TRF7964A I also would like to confirm appropriate RX Special Setting Register (0x0A) value for FeliCa.
The read back resister value after ISO Control register (0x01) setup was 0x10 for 212/414kbps FeliCa. According to data sheet, 0x10 means…
Part Number: TRF7964A Other Parts Discussed in Thread: MSP-EXP430G2ET , DLP-7970ABP Hi Andreas,
I received the LaunchPad (MSP-EXP4302ET) and am able to load an run the TRF7970ABP_RFID_Reader_Demo code, but it does read any tags.
The code seems to…
Part Number: TRF7964A I would like to confirm the following low-level resister value for FeliCa system.
*RX No Response Wait Time Register (0x07) Datasheet says that "RX No Response Wait Time Register (0x07)" is the time from the start of slot in the…
Part Number: TRF7964A Regarding main crystal(external),it seems that 13.56-MHz or 27.12-MHz crystal can be used, and the data sheet says that the 13.56-MHz or 27.12-MHz crystal (or oscillator) is controlled by the Chip Status Control register (0x00) and…
Part Number: TRF7964A Hi,
Customers want to communicate with SPI without SS. I understand that we have to use Direct Mode because TRF7964A can't use FIFO. (Errata) Is it right?
Can TRF7964A communicate with FeliCa in direct mode?
Regards,
R…
Part Number: TRF7964A HI I have designed a TRF7964A board with Microchip host controller, TRF7964A communicates with the HOST controller over SPI with SS software control, In my design I have left the I/O 5 of the TRF7964A as NOT COnnected, my board is…
Part Number: TRF7964A Hi TI Team
First of all thanks for all the Help with Hardware Design , now I have ported the "sloc297.c" code to the ATTINY Host controller, After the REQA i get an interrupt and the IRQ Status register return 0xC0. When I place…
Part Number: TRF7964A Hello. I will use TRF7964A(13.56MHzRFID). Due to Japanese Radio Law regulations, we need to do some preliminary measurements. I want to make continuous unmodulated(CW) and pseudo-noise(PN) modulated output for the RF test.
By using…