Part Number: TS3A5223 Other Parts Discussed in Thread: TMUX1237 , Currently, this IC is used as follows. One thermistor is connected to microcomputers with different drive voltages, and they are switched and used depending on the situation. For example, when…
Part Number: TS3A5223 Questions about THD of TS3A5223 Because the customer needs to use the TS3A5223 chip, we are now measuring some parameters of TS3A5223. I have some questions and ask for help. First, during the measurement of THD, according to the following…
Part Number: TS3A5223 Hi team. I'd like to know about the input voltage range for NCpin. In my customer's application,DC3.3V is always applied to NC pin when VCC=0V. Is there any problem in this case? Absolute Maximum Ratings for NC pin is 4.3V. However…
Hi Alex,
It seems 4MHz is high enough for the PWM signal. Weird~~
Is TS5A5223(TS3A5223) support Powered Off Protection? When our device power off, VDD will be droped to 0V. I am not sure if it will be affected by the AUX signal voltage which present on…
Part Number: TS3A5223 Hello
Has TS3A5223 tps max specification due to just only tplh/tphl 0.2ns (typ) &1.8V specification on datasheet? Thank you.
BR
Patrick
Part Number: TS5A4624 Other Parts Discussed in Thread: TS3A5223 , Hi,
is there a ltspice compatible simulation model for TS5A4624 and TS3A5223 available?
Best regards
Alen
Part Number: TS3A5223 Other Parts Discussed in Thread: TMUX1104 HI Team,
My customer is surveying for 1:4 mux solution supporting 1.05V signal. we found TS3A5223 is ok to meet the 1.05V need but this is 2:1 solution. Please check if TI has 4:1 MUX solution…