Part Number: TS3DV642-Q1 Hi Team,
Good day,
We are using TS3DV642-Q1 in our design to connect with Display port
We have following queries to be addressed by TI expert team.
CEC pin can be left open or else recommended to use any Pullup/Pulldown
HPD pin…
Piet
Please see this for the TS3DV642 s-parameter model.
https://e2e.ti.com/support/switches-multiplexers-group/switches-multiplexers/f/switches-multiplexers-forum/473446/ts3dv642-s-parameter-models-provided
For stackup, I sent you the board in a private…
Chengkai
CHENG KAI said: 1,What is the VCC value if the 2lane MIPI CPHY voltage is 1.8V?
VCC is minimum of 3.0V and max of 3.6V. Typically VCC is 3.3V.
CHENG KAI said: 2,How can I deal with the IIC interface-PIN3/4,PIN38/39/40/41,they all connect to SOC…
Part Number: TS3DV642
Hello. Can I use TS3DV642 chip to switch 10" LCD panel with LVDS input between two sources? How to match impedances and voltage levels? Thanks.
Part Number: TS3DV642-Q1 Hi,
A simple question to make sure I understand SEL1/SEL2 configuration correctly:
What happens for channels A and B if both SEL1 and SEL2 are high ?
Best regards,
CB
Part Number: TS3DV642-Q1 Hi,
Do you think it would be ok to have, with either an HDMI or DVI connector on the one side an HDMI and a DVI connector on channels A and B of the other side ? Apart from properly routing the different channels on both connectors…
Part Number: TS3DV642-Q1 Other Parts Discussed in Thread: TS3DV642 When I use TS3DV642 as a MIPI CHY mux with MAX96712,I have a problem- that the Ti mux just support 3lane mode CPY, but max96712 is 4lane CPHY,please see the figure below:
Part Number: TS3DV642-Q1 Hi Team,
Hope you are doing well!
In Mipi DPHY based DSI switching application, can the channels be customized? For example, the pair of pins D0+/D0- is connected to the CLK+/- of LVDS.
Part Number: TS3DV642-Q1 Other Parts Discussed in Thread: TS3DV642 , HD3SS214 Hi expert,
Do we have HDMI to MIPI(CSI)/ converter or DP MUX devices?
Many thanks to your help!
Kind Regards
Imelda