Part Number: TS3L500AE I need a IC that works similar to a SPDT relay with its coil. I mean, without power supply present, I need that "C (common)" and "NC (normally closed)" contact should be connected.
When power supply supply is…
Part Number: TS3L500AE Hi Team,
My customer want to use TS3L500AE to replace relay as following shows:
Is there any relevant application notes or information could share with my customer for reference? Could TS3L500AE be placed between the transformer…
Part Number: TS3L500AE
Hello team,
My customer is considering to use TS3L500AE between AC coupling magnetics and RJ45 connector. The purpose is mechanical relay replacement.
Please find internal link here for the block diagram. (Please connect to VPN…
Part Number: TS3L500AE 1. Is this a bilateral analog switch ic
2. Is it compatible with single ended (lvcmos25) signals also ? because my application requires both differential and single ended.
Part Number: TS3L500AE Other Parts Discussed in Thread: ADS5421 1. can it be used with cmos (2.5v) and LVDS , out of 16 bits 8 bits are LVDS and remaining 8 are cmos but to be used only one type at a time .
2. how much output capacitance it can drive…
Part Number: TS3L500AE Hi team,
I'd like to check if TS3L500AE works.
As TI doesn't provide EVM for this device, I'd like to use pitch conversion break board.
The problem here is I don't have break board which fits WQFN56P.
So, I'll use…
Part Number: TS3L500AE
Hii
will the performance of this ic (
TS3L500AE, TS5MP645 )
depend upon the output capacitive and resistive loading or it works like a mechanical switch
For example if let's say the previous buffer in the path was capable to drive…
Part Number: TS3L500AE Hi team,
My customer is considering using TS3L500AE with the two configurations shown below for 10/100/1000Base-T applications.
The customer asked which configuration is recommended for 10/100/1000Base-T applications.
I think configuration…
Hey Alvin, Welcome to E2E! So I was able to find a few previous posts on similar topics.
https://e2e.ti.com/support/switches-multiplexers-group/switches-multiplexers/f/switches-multiplexers-forum/676069/ts3l500ae-10-100-1000base-t-applications/2490709#…