Part Number: TS5A23157-Q1 Other Parts Discussed in Thread: TS5A23157 , PCA9306
Hello TI engineers,
In our PCB design, we found a BUG, when power on ,an abnormal 900mV voltage appears on the network connected to Pin 10 of the TS5A23157. In our design …
Part Number: TS5A23157-Q1 Other Parts Discussed in Thread: SN3257-Q1 Can I use in this scene: I use 1.8V for V+ , but 3.3V for IN1 and IN2. Can TS5A23157-Q1 work well?
Part Number: TS5A23157-Q1 Other Parts Discussed in Thread: SN74LVC2G66-Q1 Hello team,
Is it possible to use TS5A23157-Q1 as 2ch SPST switch, to control one more slave device to the working I2C bus line(master, slave1, slave2)?
(FYI - SN74LVC2G66-Q1 can…
Part Number: TS5A23157-Q1 Hi TI team,
we are looking for a i2C mux , below is the application block diagram
With AEC qualified,
Temperature grade: -40°C ~ 85°C
Can you please suggest a suitable part? Can we use :TS5A23157QDGSRQ1 for below implementation…
Part Number: TS5A23157-Q1 Hi TI Expert,
I notice the datasheet of TS5A23157-Q1 suggest us to use 10kohm - 100kohm on IN pins to ensure the state during startup.
May I know whether it is really necessary?
Thank you.
Part Number: TS5A23157-Q1 Other Parts Discussed in Thread: TS5A23157 My application is switching of a DC bias voltage, where the analog switch is not permitted to add a positive or negative offset.
Even an offset of 1mV will have an effect.
I'm not sure…
Part Number: TS5A23157-Q1 Hi, Support Team
TS5A23157-Q1 could support I2C for 400Khz protocols?
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: TS5A23157-Q1 Hello team,
My customer has related questions about TS5A23157-Q1 as below, could you please give a detailed explain about each condition.
(1) If the V + power supply is 3.3V and the input and output signal (no, NC, COM) level…
Part Number: TS5A23157-Q1 Other Parts Discussed in Thread: TS5A23157 Hi Team,
Recently, during customer's PV experiment, customer found that the TS5A23157DGSRA package bulged and failed as following picture.
What kind of problems or conditions will…