Part Number: TS5A23159 Hi everyone.
I have a design use TS5A23159DGST as attached file. I also use ESD5581N2T5G to protect I/O pin when I connect them with external peripheral device.
I have tested this PCBA FCT, they are working without any problem, but…
Part Number: TS5A23159 My circuit requires to switch the USB-C port between some ICs. In order to do so, I came up with two TS5A23159DGSR behind each other. Selected via a DIP switch to ground or VCC. Just wanted to check, if this is a solution that should…
Part Number: TS5A23159 Other Parts Discussed in Thread: TS5A23157 , , TS5A623157 Hi,
Can the TS5A23159DGSR be used as an IIC switch? It is assumed that two master devices are used by switching for a Slave Device.
In that case, the power supply of TS5A23159DGSR…
Part Number: TS5A23159 Other Parts Discussed in Thread: TIDA-00879 , TMUX6236
Hi there,
I am using this switch to sense a voltage drop across a resistor similar to a TI multimeter application (TIDA-00879). My question relates to exceeding the Vnc, Vno…
Part Number: TS5A23159 Dear Sirs,
My customer use 5V for Vcc and found, if the input signal is 3V, the power consumption will more than 5V signal input!
May I have your help to provide IC internal block data and(or) explain why this symptom happened?
…
Part Number: TS5A23159 E2E,
I'm looking at the TS5A23159RSER switch and had a question about its off-isolation. Can you please confirm that it is okay to apply 1.8V to NC, NO, or COM even when VCC = 0V? It looks like worst leakage in this case is…
Part Number: TS5A23159 Other Parts Discussed in Thread: TMUX136 Hello Expert,
Our customer has already been using TS5A23159, TS5A4624DCKR on their product.
So they want to use this part for USB 2.0 data instead of USB protocol-specific switches & muxes…
Part Number: TS5A23159 Hi Team,
I have a question about TS5A23159, can TS5A23159 replace FSA2257? Here are some information about FSA2257. FSA2257 is one of chips in Fairchild.
BR
Gust
Part Number: TS5A23159 Dear Team,
There is a good news that we DIN TS5A23159 in our customer.
Could you help to review the schematic as below?
We appreciated your great support!
Many Thanks,
Jimmy
Part Number: TS5A23159
The Datasheet specs C NC(ON) , C NO(ON) , C COM(ON)
[1] Assuming a signal gets routed from [Host] -> [NO->COM] -> [Device]; will the signal see rise-times that relate to the combined C NO(ON) + C COM(ON) ?
[2] Basically, the bus capacitance…