Part Number: TS5A3159A Other Parts Discussed in Thread: SN74LVC1G3157 Hi team,
customer has a 3.3V 4MHz and a 1.8V 37.125MHz clock signal need to switch. I was wondering if TS5A3159A can work here. If not, any recommended device for it?
Rayna
Part Number: TS5A3159A Hi Team,
Could you pls check the Storage temperature of this device? Are the temperatures the same for different packages? Thanks!
Regards, Hailiang
Hello Renan,
The supply current should be 5 nano-amps for the 1.8v . Also the graphs in the datasheet should be nA range. We will make these updates to the datasheet soon.
Thanks and Regards,
Kameron
Part Number: TS5A3159A I have two power supplies that are always on, 1.8V and 3.3V. I would like to determine if this part is suitable to operate on the 3.3V supply and switch the common between 3.3V or 1.8V (SPDT). The common current is about 20ma to…
Part Number: TS5A3159A Team,
My customer used TS5A3159A as switch, which input signal is AC coupling signa. Needs to check with you if TS5A input can be AC coupling.
Thank you!
Part Number: TS5A3159A Hello,
When a customer order for example TS5A3159ADCKR, how can they know which dimensions they are getting? There are two option with identical part numbers but different lead dimensions. How do we differentiate?
Thanks
Jo…
All,
The absolute maximum conditions of the device must be respected at all times. Failure to do so can result in abnormalities in signal integrity when powering up/down the device while having analog signals present on the device channel, or could result…
Part Number: TS5A3159A Hi Team,
My customer use 100k ohm resistor but they found that the discharge speed is too slow cause sequencing problem. So, we would like to check if we can decrease this resistor value because we don't see the recommended value…
Part Number: TS5A3159A
Hi team,
My customer noticed that TS5A3159A has a function of Isolation in Power-Down Mode. This means its COM/NC/NO pin can accept signal when the device is powered off without damaging the device.
But my customer wants to know…