Part Number: TS5V330 Other Parts Discussed in Thread: TS3V330 Team,
I have a customer looking to switch between 3 different NTSC/composite video channels to a single output. I see you have the TS5V330 series which is a 2:1 MUX for composite video, but…
Hello Eduardo,
It would be better to go up rather than down in resistance. Since this is a current feedback amplifier, RF has a large effect on the stability of the device. While lowering the resistance may add more ringing (probably not enough to go…
Eduardo, I think you may be right. Good luck with this and I hope it works properly with the new part! In the meantime, i'm going to close this thread but don't hesitate to reach out and update me if any new information or problems arise. Thanks…
Part Number: TS5V330 The chapter 4 in the application note SLOA040, page 7 , specifies the SMA adapters for differential gain and phase. Normally a SMA connector has 50-ohm impedance, while the NTSC trace on a PCB has a 75-ohm trace. Will this impedance…
Hello Kuramochi,
A quick response for your question is yes, you can use any of our analog switches for National Television System Committee signals, so long as the switch matches their bandwidths and voltage levels.
Please refer to the link of a previous…
Part Number: TS5V330 Hello Team,
Customer reports that the output from TS5V330PW is clipped at 4.1V with the following conditions:
VCC=5V
Vi=5V
In general, when Vi>4.1V the output is clipped at 4.1V. Is that expeced?
Does this depend on the current…
Other Parts Discussed in Thread: TS5V330 Hello Team,
I would like to ask you about TS5V330.
I have posted this thread in Signal switch forum.
http://e2e.ti.com/support/interface/etc_interface/f/388/t/360563.aspx
I posted this thread in High speed interface…
Other Parts Discussed in Thread: TS5V330 Hello Team,
I would like to ask you about TS5V330.
My customer assumes the use of TS5V330 in the following figure.
Can my customer use TS5V330 as shown following figure?
(Both RGB and Y/PB/PR needs to correspond to…
Adam,
thats the limitation of our current design. We can either use input voltage which is up to 28V or use voltage after converter which is 4.5V.
I'm thinking of going with this one in the end: TS5V330.
What do you think?
Cheers,
Sergey
Part Number: SN74CBT3251 Other Parts Discussed in Thread: SN74CBT162292 , SN74CBT16292 , SN74CBT16232 , SN74CBT16390 , SN74CBT3257C , SN74CBT3257 , TS3V712EL , TS3V713EL , TS5V330 , TS5V330C Hi Sir
May we know if SN74CBT3390 already obsolete?because i can't find…