Hi Bhaeddin,
I will check this issue with the design team and learn there feedback. If they could not get any reasonable explanation, I will try the test in the lab.
Please allow me time to do that. Meanwhile can you post the same query on a separate…
Part Number: TSW1265EVM Other Parts Discussed in Thread: LMK04808 , Hello, I use a TSW 3085 as Tx and a TSW 1266 as Rx. Following the example of evaluate madule and using LMK04808_614p4M_Single_Loop.txt. in TSW 1266 GUI I had a good result in the Rx as shown…
Other Parts Discussed in Thread: TSW30SH84EVM , TSW1265EVM Hi,I have TSW1265EVM and TSW30SH84EVM.I want use TSW30SH84EVM clk6p output as TSW1265EVM clkin input.If the divider is 12,then clk6p is 2949.12/12=245.76MHz.
My questions is
1. Which CLK0 type should…
Other Parts Discussed in Thread: TSW1265EVM , ADS4249 Hi TI,
TSW1265EVM this part no can i digitize the analog signal input to the board with following spec...
1. IF: 60MHz
2. Input max limit : +12dBm
3. Dynamic range : 100dB
The range should be 100 DB…
Other Parts Discussed in Thread: TSW1265EVM Hi,I let my foreign friend buy tsw1265evm and tsw1266evm for me.I get the box today,but I only find the board and USB cable in every box. There are no power supplies in them.Please tell me what can I do? I need…
Other Parts Discussed in Thread: ADC12D1800 , ADC12J4000 , TSW30SH84EVM , TSW1265EVM
Hello,
What’s the cheapest solution for a Ready board (without the need to edit any PCB) which includes ADC-FPGA-DAC for having an FFT of at least 500MHz IBW? (i.e. sampling…
Hi,I let my foreign friend buy tsw1265evm and tsw1266evm for me.I get the box today,but I only find the board and USB cable in every box. There are no power supplies in them.Ken.c had agreed to ship them to me.I had send address to Ken.c,but no one contact…