Part Number: TSW1405EVM Other Parts Discussed in Thread: AFE5809EVM Hello,
when I evaluated afe5809evm using tsw1405evm, I found that only ‘1W_SERIAL.SVF’ is available in the firmware. Now I want to develop a new firmware for myself to use. Who can…
Hi Mariusz,
We do not have TSW1405EVM firmware that is compatible with the ADC3441EVM at the moment. This feature may be added at a later time, but I do not have an exact date.
Best Regards,
Dan
Part Number: TSW1405EVM We have a data capture card TSW1405evm. Is it possible to measure 8-bit Single Data Rate (SDR) ADC with this evaluation module. In other words, is it possible within the High Speed Data Capture Pro to change type of input signal…
Part Number: ADS41B49EVM I have two hardware,one is the ADS41B49EVM,and the other one is TSW1405EVM. I have already installed ADC SPI and HSDC GUI. However, I give clock (20Mhz , Vp-p1.5V )and give sine wave(50Mhz, 1dbm ) to J6, I can't see anything on…
Sergey,
I have attached a copy source code for the TSW1405EVM that I could find from the engineer that use to support this.
Regards,
Jim
TSW1405 EVM Firmware.zip
Part Number: TSW1405EVM Other Parts Discussed in Thread: DAC3482 I use a TSW 1405 to generate a signal and a TSW 1406 to receive. I read the example in the documentation and I generate a signal out of my expected frequency using the frequencies of the…
Part Number: TSW1405EVM Other Parts Discussed in Thread: TSW3085EVM , TRF3705 Hello I am in need of more detailed documentation on the TSW 3085 EVM and the TSW 1266 EVM. I was able to send and receive an example signal based on the documentation from…
Part Number: AFE5809EVM Other Parts Discussed in Thread: AFE5808AEVM , We are trying to interface AFE5809EVM with TSW1405EVM . Where can we find the ini file required for HSDC Pro GUI?
Part Number: TSW1405EVM Other Parts Discussed in Thread: AWR1642 Hi All,
I was wondering if it is possible to capture raw data from AWR1642 using TSW1405EVM without the mmWave DevPack Board.
Raashid