Part Number: TUSB1064 Hi,
I have an Application for Display port and USB port, the USB should work in Device mode(ex: Flashing),at that time The Display Port Should be Active(like both usb & DP work Concurrently)
for this application I have a SOM…
Part Number: TUSB1064 Dear
my item is related to the document Circuit Protection for USB Type-C - Literature ID slyy105.pdf
The customer wrote the following:
referred to a following details below. These are described that the Vbus can cause a short circuits…
Part Number: TUSB1064 HI team,
TUSB1064 only has 2 lanes when switching U31 signals. Do we have a newer solution to switch 4 lanes of USB and 4 lanes of DP, which means 4 in 8out?
Thanks
Lillian
Hi,
Are you able to solve this issue? I will go ahead and close this thread for now, but you can reply back to this thread if you have any update.
Thanks
David
Part Number: TUSB1064 Dear E2E teams,
i use TUSB1064 for Typec to DP project.
TUSB1064 and DP receicer IC is on one board, so there is not DP Hot plug.
i pull up HPD of TUSB1064 with 4.7K all the time, is this OK?
thanks!
Hi David,
Thanks for your support.
We got TUSB1146EVM and TUSB1064RNQEVM and will give it a try.
To learn about the max length of USB type C cable when it transmit a 720P video.
Regards
Eric Li
Part Number: TUSB1064 David-san
sorry to have kept for a long time.
I tried to check the swing level by differential probe again by using several laptop and desktop.
when I measure again it,
the swing level after TUSB1064 was increased.
I'm not sure…
Part Number: TUSB1064 Hi Team,
I need IBIS models for this part? I would like to simulate the TX and RX lines in a HyperLynx board simulation. could anyone please provide that?
Thanks
Narsimha
Part Number: TUSB1064 To compare TUSB1064 datahseet(page 32) and document(HSDC025A-002 Schematics.pdf), it shows different capacior value on USB TX/RX path
Attchement is our functon block, please advise the ac capacitor value(red color ellipse)
[Problem] decrease the swing of AUX after pass through TUSB1064_rev4.pptx
David san
sorry, moreover from above message,
let me update the information.
I measured swing voltage level for each section of AUX.
please refer to ppt slide and give us comment…