Part Number: TUSB2036 Other Parts Discussed in Thread: TUSB8020B I use this device to split USB2.0 from a USB3.0 signal ( I need one USB3.0 to ethernet + one USB2.0 come from a USB3.0 port).
I think The PC is seeing my board as a USB1.1 hub .
Because…
Part Number: TUSB2036 I used " TUSB2036VFRG4" hub with 6GHZ crystal. the speed of the USB port is 12MB/S.
I think I need to go with 48 MHZ clock to get the full USB speed. AI right?
Do anyone has a recommendation circuit to create 48 MHZ clock? …
Wayne:
Sorry for the delay, since this device was designed 20 years ago,it took some time for design to find the database.
This is the block diagram for crystal oscillator. The GZ port controls the oscillator's functionality. GZ can disables the oscillator…
Part Number: TUSB2036 I've been tasked with a project at work that is fairly outside my scope of knowledge and hoping others might have any potential advice.
Is it possible to communicate with a TUSB2036 USB chip to poll if a port is actively providing…
Part Number: TUSB2036 Hi,
I am using TUSB2036 to split USB connectivity into 3 USBs. I took as a refferance datasheet and "USB 2.0 EMC Stick with integrated ESD Protection and EMI Filter" [1] from Wurth Electronic to add protection filter to the input…
Part Number: TUSB2036 Hi All,
Customer is using TUSB2036 between CPU and USB memory connection.
An event that cannot write or read has occurred when connecting the CPU and USB memory.
The connection is often failing when opening the file. Also, using a…