Part Number: TUSB2036 Other Parts Discussed in Thread: TUSB2046I Hi,
The customer is considering a TUSB2036VF. However, we want a wider temperature range, so we are looking at the possibility of replacing it with a TUSB2046IBVF.
1. By connecting 21 to…
Part Number: TUSB2036 Brian,
OK, so it's best that I choose another hub IC. Which would you suggest?
requirements:
- 3 port
- USB2.0
- based on the new USB phy
- footprint size comparable to the TUSB2036 ( TQFP32 or QFN32, ... )
Thanks.
Best regards…
Part Number: TUSB2036
If possible, I would appreciate it if you could take a look at the attached schematic and give me some advice. Currently, we have built a circuit using your product TUSB2036VF, but this device works at low speed, but not at full…
Part Number: TUSB2036 If possible, I would appreciate it if you could take a look at the attached schematic and give me some advice. Currently, we have built a circuit using your product TUSB2036VF, but this device works at low speed, but not at full speed…
Hi, I'm the creator of this topic and I'm finally able to post myself on the forum.
Thanks for your help Brian. I have everything I needed to know now.
Part Number: TUSB2036 Hi,
I used the TUSB2036 to connect two downstream port to the CPU. In the last version, I forgot the 15K pull down resistors. With manual assembly of these resistors, the problem resolved. I made a new version of PCB, but now the…
TUSB2036 is FS hub.
Since it's working after removing TUSB2036, can you take waveform with wired keyboard with the baord removing TUSB2036?
Regards
brian
Part Number: TUSB2036 Other Parts Discussed in Thread: TPS2043B
I have used this pair fo components as recommended by the datasheet to add some extra USB ports to my embedded linux system (schematic below)
There have been difficulties in getting this…
Part Number: TUSB2036 When 3DConnexion Spacemouse connected directly to computer, respons is normal when rotating a 3D object on the screen, without any hicks. When the Spacemouse is connected through the TUSB2036, the object rotates slowly and intermitting…