Part Number: TUSB217-Q1 Other Parts Discussed in Thread: TUSB212-Q1 , TUSB217 , TUSB212 Hi Application Team:
We would like to use TUSB217-Q1 replace TUSB212-Q1 since USB2.0 SI on Type A port of C car is too weak to pass USB IF ,
we would like to know what…
Part Number: TUSB215-Q1 Other Parts Discussed in Thread: TUSB217-Q1 , , TUSB217 , TUSB215 Hi, We used to use tusb217-q1, but for some reasons, we now replace it with tusb215-q1. However, the following problems occur when using tusb215-q1. Please analyze what…
Part Number: TUSB217-Q1 If a TUSB217-Q1 detects it has an I2C bus connected will the part still set the registers based on resistors connected to the RX_SEN and BOOST pins.
The datasheet seems to imply that the RX_SEN and BOOST pins would be ignored if…
Part Number: TUSB213-Q1 Other Parts Discussed in Thread: TUSB217-Q1 , TUSB216-Q1 , TUSB217A-Q1
Our customer is looking for re-driver for their Automotive USB Charger application to meet CarPlay / Android Auto .
Is your recommend IC TUSB213-Q1 and TUSB217…
Part Number: TUSB215-Q1 Other Parts Discussed in Thread: TUSB217-Q1 , TUSB217 , TUSB215 , TUSB216-Q1 , TUSB216 , TUSB216I Hi experts,
TUSB217RGYRQ1 was design win on customer side. Due to the supply issue, they start to evaluate TUSB215-Q1. Can TUSB215-Q1…
Part Number: TUSB217-Q1
HI Team,
We have some customers using TUSB217-Q1 that car OEM request DP/DM short to VBUS=5V protection.
When DP/DM short to VBUS=5V, would these pins or the chip be damaged ?
Thanks.
Part Number: TUSB217-Q1 Other Parts Discussed in Thread: TUSB217 Hello Team,
I got a question from customer about TUSB217-Q1.
Q. Can the I2C support fast mode(400kHz)?
Q. Is there any restriction about I2C which we should be take care?
Thanks,
Yuta K…
Part Number: TUSB217-Q1 Hi,
Because the working voltage provided by our circuit to tusb217-q1 is not fixed, the range is 2.75V ~ 3.85v, and the voltage will change with the product working temperature (± 0.2V). Do the gain/sensitivity and other states…
Part Number: TUSB217-Q1 Other Parts Discussed in Thread: TUSB217EVM Hi team,
does the TUSB217-Q1 have USB-IF authentication, Can you share the report? thanks.