Sounds good. I am going to mark this thread as resolved, but feel free to reopen it if you run into issues related to this thread.
Kind regards,
Conner Gillette
Part Number: TDA4VM Hi Team,
Single board silkscreen J721EXSJG01 EVM to boot Linux or RTOS operating system from SD card with serial interface information as follows:
COM1: Information is printed, only Hex values, but cannot be entered
COM2: No information…
Part Number: AWRL1432BOOST Other Parts Discussed in Thread: SYSCONFIG Hi, TI Team,
I run the MCAN External Read Write example on my xWRL1432 evm following the instruction as the link below. But PCAN has Bus warning after PC sent a CAN FD message to EVM as…
Hi Xulin, Estimating the effort in debugging and identifying the root cause, the current plan from TI is to target for a fix in SDK 9.1. I checked internally, and currently there are no plans to provide an intermediate patch.
I shall get back to you if…
Ricky Lau said: Are you using AM64x and AM243x via UniFlash GUI?
Yes, I was using the GUI. The Uniflash GUI recognized the board and listed it correctly. When I select a board, it responds the same with AM64 and AM243. But when I attempt to load/run an…
Part Number: MMWCAS-RF-EVM Hi team,
Here's an issue from the customer may need your help:
1) A 2-m roof was measured as a calibration matrix, and this echo data was processed using cascade_MIMO_antinnaCalib.m after calibration, using cascade_MIMO_signalProcessing…
Part Number: TDA4VH-Q1 Other Parts Discussed in Thread: SK-TDA4VM , AM69 , SK-AM69 , TDA4VH
Hi,
Do you have a TDA4VH-Q1 EVM which has a 12-layer or 10-layer stackup like SK-TDA4VM?
The current TDA4VH-Q1 EVM https://www.ti.com/tool/J784S4XEVM has a 16…
Part Number: UCD90120 Other Parts Discussed in Thread: UCD90SEQ64EVM-650 Hi Experts, We received 20 devices with package marking TI 28I CJEH G4.
I am able to program multiple times the 1st device with TI Fusion 2.0.179. NVRAM programming is happening…