Part Number: TUSB4041PAPEVM I saw in a previous thread that there is no way to make use of the EEPROM Programmer Tool as a CLI. In yet another thread where I received help, there was mention of using the T otal Phase Control Center Serial Software to affect…
Part Number: TUSB4041PAPEVM
Hello,
I'm using the TUSB4041PAPEVM evaluation board together with "TUSB80xx_EEPROM_Programmer_V1.0.0.1" toolkit
The EEPROM was empty (0xFF) from delivery and I have know made my unique configuration file to…
Part Number: TUSB4041PAPEVM
Hi !
We got the evalutaion module and like to test the EEPROM Windows toolkit, where can I find and download it ?
Rgds,
Ola
Part Number: TUSB4041PAPEVM
Hi,
We got 3 different USB2 dongles attacted to this module for evalutaion to a coming custom board.
Since both the EVB module and the dongles can be fed from VBUS (Bus power) with USB2 restricted to 500 mA I was wondering…
Part Number: TUSB4041PAPEVM Hello!
Could you confirm that the EEPROM part recommended is the 24AA04-I/P? This is what is listed in the BOM, but on the schematic it is labeled as AT24C04.
Thanks,
Sarah
Part Number: TUSB4041PAPEVM Hi, do you know if two TUSB4041 connected with a 5m USB cable can comply 1kV Signalburst Test with Criteria B ?
(CritB: after the burst disturbance the connection should be reconnected without user action)
BR Martin
We have been able to reproduce the issue in 4 different systems. This should show that it is not dependent on the USB host controller. Same hub disappearing and re-enumerating issue is observed with four different system and hosts: 1. Intel Core i7 laptop…