Part Number: TUSB542EVM Other Parts Discussed in Thread: TUSB321 dear
customer bought the sample development board for TUSB542EVM, and tested it with the board. The configuration mode of the original board is DFP mode, type-b is Host, and type-C is…
Part Number: TUSB542EVM Other Parts Discussed in Thread: TUSB542 Hi Team
Does void under coupling capacitors and pads of connector and TUSB542 is must ?If we we keeping void then it should be
only on next layer or how it should be ?
Nishie-san
Figure 23 was copied from the TUSB542EVM.
The large holes are for mounting stand to the EVM.
The small holes are fiducial mark. A fiducial mark is typically a circular pad or other shapes of exposed copper that is surrounded by a clearance area…
Part Number: TUSB542EVM Other Parts Discussed in Thread: TUSB542 Hi Team, There is different pin assign between datasheet and EVM as the following. -------------------------------------------------------- - TUSB542 datsheet -TUSB542EVM --------------------…
Part Number: TUSB542EVM Other Parts Discussed in Thread: TUSB321 , TUSB542 , Hi
Can i use this EVM connect in this way "Connect the Type C to the PC and the Type B to the device " ?
Thanks!
PY Tsai
Dear David,
Thank you for your support.
Here is another question.
As a result, my customer drew their schematic based on TUSB542EVM, and they just changed TUSB542 to TUSB1044. (and changed USB A to type C)
I think it will be working as USB3.1, just give…