Part Number: TUSB7320 Brian Zhou has replied to a thread: RE: TUSB7320: Cannot connect USB 2.0 devices(Additional question)
I want to unsubribe from this email
Hi Brian,
Brian Zhou said: For question 1: It's known issue to have errors when transferring balk files for Linux system. Can you check with linux community too?
I have no experience about linux community. Could you help give any url about TSUB7320…
Part Number: TUSB7320 Please tell me about the revision of the TUSB7320 data sheet (Rev.M → Rev.N).
VDD11 power supply accuracy changed.
1.1V±10%=>1.1V −5% / +10%
Please tell us the background.
Regards,
Part Number: TUSB7320 Hi,
I am looking for the BSDL file for the the TUSB7320. At the moment we have a problem with testing a jtag chain where the TUSB7320 is in line with two other devices. Bypassing of the TUSB7320 fails, maybe our current bsdl file…
Part Number: TUSB7320 Can any electrically-valid behavior of a connected USB2 device cause a permanent failure of the TUSB7320 USB Host Controller?
One of our PCI Express card designs has the TUSB7320, without a configuration EEPROM installed, with a…
Part Number: TUSB7320 I know the chip is old but it's the only thing available so I'm using it in a new design. I seen mention of a "eeprom programming tool" and a "template". I have an external programmer so I don't think I need the tool, but I could…