Hi Rajat Rao ,
Yes, this is correct. VIP just works based on the information available from TDA5158, especially in multiple channel mode. So please make sure that TVP5158 is configured correctly. Btw, which mux mode are you using? Can you please make…
Part Number: TVP5158 Hi All,
I have a question about TVP5158.
It is stated that analog clock multiplier PLL is supplied as a reference from the outside.
Are there any other input signal factors to generate the system clock output (An analog clock multiplier…
Part Number: TVP5158 Hi Team,
There is a good new that we could DIN TI product!
Customer is looking for the Video Switcher !!!
1. Does our device "TVP5158" ever been used for video signal switching between HD-TVI and SD-CVBS?
2. Do we have design…
Hi Rajat,
Please check the VIP instance that you are using and from TRM, you could get the base address of this VIP instance. Please save 100 registers from this base address and share them.
Regards,
Brijesh
Part Number: TVP5158 Hi Team, May I ask for help? I am not quite sure if this is the right forum to ask but our customer have a concern below:
Looking for semiconductors associated with designing an analog 1x 6 composite video distribution amplifier. There…
Part Number: TVP5158 Hello TI Team
In our Product we are getting input from Four camera as Monochrome Interlaced Video (RS-170 ) which support NTSC/PAL; Need a 4 channel, 8 bit decoder of BT656
We got TVP 5158 IC with 4 channel ADC video decoder NTSC/PAL…
Part Number: TVP5158 Dear Champs,
Our customer ask us below problems, could you kindly give us some suggestions:
How long is the latency between the analog signal input to the TVP5158 and the data output?
When TV5158 generates images, will it use past…
Part Number: TVP5158 he schematic diagram of the attachment supports 8-way video input, as shown below. Please confirm whether it is simultaneous 8-way video input or time-sharing 8-way video input?
That is to say, whether the two Ti 5158 chips do real…
Part Number: TVP5158 Tool/software: Linux Hi team,
My product is 4-Ch Line-Interleaved Mode, and 4-Ch Half-D1 Format, thus, OCLK is 54 MHz.
However, I measured the OCLK_P waveform, then, the waveform is a Sine-Wave instead of Square-Wave.
My question is…