Part Number: TVS0500 Other Parts Discussed in Thread: TPS25947 , TVS1400 Hi,
I used TPS25947 in input and only support to minimum -15V negative voltage protect.
If I want add TVS to increase negative protect range, Could I add reverse uni-direction TVS…
Part Number: TVS0500 An IEC61000-4-4 Burst Noise test was performed on the cabling connecting to a board with a Δ∑ADC. The cables connect to the board and PCB traces take the signals to the ADC, through an input CM / Diff filter.
Right now there…
Part Number: TVS0500 Other Parts Discussed in Thread: TPD1E10B06 , Hi,
Let me ask you a basic question about TVS0500 and TPD1E10B06.
About the failure mode of both devices in the forward or reverse direction, an open failure or a short failure?
Thank you…
Part Number: TVS0500 Other Parts Discussed in Thread: ESDS312 A 1-Wire network of devices has a requirement to withstand signal to ground surges described in IEC 61000-4-5, level 2 for unshielded, unsymmetrical data lines.
The devices have a max voltage…
Part Number: TVS0500 Are there any Reference Designs / Schematics / examples floating around somewhere, for using such TVS protection devices for IEC 61000-4-4 EFT noise protection?
Sizing external series resistor, etc...any design guide? I can't seem…
Part Number: TVS0500 Hello
We have a requirement to insert a voltage drop in a circuit that must withstand 1.5A (maximum and non-repetitive) for a few 10s of milliseconds. The data ( SLVSED2C, Figure 2) shows the TVS0500 will clamp to 8 to 8.8V in this…
Part Number: TPS259824OEVM Other Parts Discussed in Thread: TPS25982 , TVS0500 In this EVM, include TPS25982's design calculator, the recommended input voltage clamp diode is SMCJxx, as TI has its own TVS diode, such as TVS0500, etc. May I use them? Thanks…
Part Number: TVS0500 Hi teams
I have few questions about select a right TVS for eFuse protection circuit. Below is a simplify SBD of my system.
The output of eFuse will power the DC-DC which have 6V maximum voltage tolenrance.
The rated input voltage…
Part Number: TVS0500 Hey, we are integrating this part with our Board. So we were doing pre-simulation to ascertain its usage. As a part of pre-sim we attached the PSPICE transient model provided in Design & Development section to the testbench and…