Part Number: TVS1400 Other Parts Discussed in Thread: SN65HVD230 Hello,
Would the TVS1400 protection device be a good fit to protect a SN65HVD230D working at 1Mbaud ?
Breakdown and clamping voltages seem to be adequate.
I need the SN65HVD230 protected…
Part Number: TVS1400 Other Parts Discussed in Thread: TVS0500 , TVS0701 , Hi,
In my earlier post i had raised the below query
Planning to use TVS1400 on 12V DC line and TVS0500 on 6.2V DC Line. Since on TVS0500 VRWM is 5V, but the Clamping voltage is 9.2V and…
Part Number: TVS1400TVS1400DRVR is used on the power line of the power connector (hot plug).
When the power is turned on with the hot plug, the inrush current will increase if the TVS1400DRVR is used.(As much as with a 1uF capacitor)
When the TVS1400DRVR…
Part Number: TVS1400 Other Parts Discussed in Thread: TVS0500 Hi,
Planning to use TVS1400 on 12V DC line and TVS0500 on 6.2V DC Line. Since on TVS0500 VRWM is 5V, but the Clamping voltage is 9.2V and the Vbris around 7.7V Are my part selection OK
Regards…
Part Number: TVS1400 Other Parts Discussed in Thread: TVS0500 Hi,
Planning to use TVS1400 on 12V DC line and TVS0500 on 6.2V DC Line. Since on TVS0500 VRWM is 5V, but the Clamping voltage is 9.2V and the Vbr is around 7.7V Are my part selection OK
Regards…
Part Number: TVS1400 Other Parts Discussed in Thread: TVS3300 , TPD2E007 , TVS2200 , , TVS0500 TVS1400DRVR& TVS3300DRVR is single channel or three channel EST protection part? We found the part pIn4,5,6 short together.
If single channel, why not use one…
Part Number: TVS1400 Other Parts Discussed in Thread: TPS24750 Hi All,
I am checking TVS1400 as a replacement to SMAJ12A-E3/5A. This TVS is placed after TPS24750 + CSD16570Q5BT reverse current blocking FET. TPS24750 does not allow below -0.3V at its output…