Part Number: TVS1401 I'm trying to use Pspice for TI to model some behavior with the TVS1401 for an ADC. (Basically trying to copy this: https://www.ti.com.cn/cn/lit/an/sbaa547/sbaa547.pdf )
Can somebody sent me a "PSPICE for TI" project file that is…
Part Number: TVS1401 Hi Andy,
My customer need to know the factor of Steady "State Power Dissipation" which is not shown in the datasheet. Could you please kindly advise it?
Thanks a lot.
Vincent Chen
Part Number: TVS1401 Hi Team,
My customer is considering use TVS1401 in PLC AI application, the leakage current will affect the system's accuracy. We can find the leakage current plot at 14V reverse working voltage but in real operation the working voltage…
Part Number: MAX3223E Other Parts Discussed in Thread: TVS1401 Hi,
My customer want to have RS232 transceiver with supporting Vrx > 36V, currently MAX13223E could support this requirement.
May I know whether TI have similar part?
According to TI cross…
Part Number: TVS1401 It is not clear what the status of the TVS1401 is. The data sheet shows a PTVS1401 as active and the TVS1401 a preview. But, I cannot find the PTVS1401 in the TI system and no vendor has the TVS1401.
If the TVS1401 is in development…
I previously posted this related support question ( https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1269261/bq24074-safe-usb-c-input-protection-ptc-tvs-diode )
I made a prototype using the TVS1401 + PTC as shown…
Part Number: BQ24074 Other Parts Discussed in Thread: TVS1401 Hi,
I've used the BQ24074 and I'd be grateful if someone could take a look at my schematic to see if there's anything that looks incorrect.
I've read the documentation available…
Hi Hao,
The XTR111 error flag is able to detect the open-circuit, wire break, or high load resistance when the output voltage of the XTR111 approaches the VSP=19V supply. The XTR111 output compliance voltage extends at least 2V from the supply (at least…
Hi Parker,
I found a TVS that seems suitable, but it is a bit pricey. Semtech TCLAMP1202P. According to their datasheet I would need 3 of these guys. I'm not sure this is any better than using the thyristor + TBU + TVS approach that I see everywhere.…
Hello Inho,
TPD2E007 has both ESD and surge protection capabilities. If you look at the datasheet, you will see two standards listed: IEC 61000-4-2 (ESD) and IEC 61000-4-5 (surge). For surge, this device is rated to withstand up to 4.5 A of surge current…