Part Number: TVS1801 Other Parts Discussed in Thread: TCAN332 , Hi Sirs,
We have use TI TCAN332 and we would like survey ESD protect on CANH、CANL .
Does TVS1801 is suitable solution?
TCAN332 specification 8.1 mentions that the maximum can withstand -14~…
Hi Grady,
1. The TVS1801 will be a good fit here since the SMBJ16CA has a bi-directional polarity. It's offered in the DRV package (2.00mm x 2.00mm)
2. I'm not aware of any direct conversion formula for 8/20uS to 10/1000uS peak pulse ratings. The…
Other Parts Discussed in Thread: ULN2003B , TVS0500 , TVS2200 Hi,
Good Day. I would like to confirm if the devices below can support 230V AC line surge protection for PWM Power Supply Unit.
https://www.ti.com/product/TVS1801
https://www.ti.com/product/T…
Hello Inho,
Unfortunately, we do not have any devices with an 18 V Vrwm who's primary function is ESD suppression. However, you could protect the 18 V power line to the amp from surge using a TVS1801, if you don't have a surge protection device already…
Part Number: UCC39002 Other Parts Discussed in Thread: TVS1801 Hi Team,
My customer is designing the UCC39002 application, asks us about ESD protection for LS pin of UCC39002. In case of their system, one power board has one UCC39002, and LS pins of UCC39002s…
Hello Hao,
Thank you for your reply.
I understand clamp voltage is around 17V.
I have another question.
TI has flat clamp surge protection device which is based on FET solution. (like TVS1801)
In THVD1429, Is this TVS solution same as FET solution like…
Hello John,
you can take a look at the TV1801 surge protection device to prevent Vbat input voltages above 18V :
http://www.ti.com/product/TVS1801
In addition there is a training video "How to Design Protection Circuits for Analog I/O Modules"…
Part Number: TVS2700 Other Parts Discussed in Thread: FLAT-CLAMP-TVS-EVM
One of my customers was recently looking for TVS diodes to protect their system from surge events, and they came across TI's TVS flat-clamp devices, particularly the TVS2700. They…