Part Number: TVS2200 Hi team,
we need I-V curve to show our dynamic resistance to customer,
datasheet only have large scale.
we need a curve around same scale as below one, please support this thanks
Part Number: TVS2200 HI team,
1.can I see surge protection device as the ESD device but with very low dynamic resistance?
2.and why type-C power line recommended add a surge protection but data line normally don't?
Part Number: TVS2200 Other Parts Discussed in Thread: TVS3300 , The maximal voltage rating of flat clamp device available now is 33V (TVS3300). Can I use 2 TVS2200 in series to form a up to 44V level surge protection device?
Part Number: TPS65994AD Other Parts Discussed in Thread: TPS65994 , TVS2200 Hi,
How close should TVS2200 be placed at TPS65994/VBUS pin? Does it need to be very close? What is the side effect if it's placed close to the type-c connector instead of TPD65994…
Part Number: TVS2200 Hi team,
As TVS2200 is a recommended solution to work with TI PD controller especially in PC market, customer would like to know how should they design the experiment to verify TVS device is working? Is there a typical test standard…
Part Number: TVS2200 Other Parts Discussed in Thread: TPS65988 , TVS0500 Hi Sir,
As the title, customer are using the original part with Amazing Microelectronic TVS "AZ2015-01H", could we replace it instead by TVS2200?
Please help to review it…
Hello Jeff,
I reviewed your project file and schematic, and I didn't see any other obvious issues, besides the missing TVS2200. I recommend adding the TVS2200 to your design, it is used to protect the VBUS pins from high voltage spikes, and I think this…
Part Number: BQ24074 Other Parts Discussed in Thread: TVS2700 , TVS2200 , TVS1401 , TPD1S514 Hi,
I need help to choose a TVS diode to protect a BQ24074. I'm not sure what clamping voltage is required.
I am making a small bluetooth household consumer electronics…