Part Number: TVS2201 Hi TI Team,
We are planning to use TVS2201 in our design to protect against ISO7637-2 pulses ( Pulse1, 2a, 3a, 3b only)
I could not find following parameters in datasheet, can you share
1. Graph with respect to Pulse with(td) and peak…
Part Number: TVS2201 I'm using the above part in my design and would like TI to review the design. I prefer email or personal messages instead of sharing in the forum.
Part Number: TVS2201 Hi,
On the datasheet, the layout example is showing connector input at pad/pin 4 of the footprint and the protected input at pad/pin 1.
What if on my layout, I have it the other way round, for example, connector input at pad/pin 1…
Part Number: TIDA-010249 Other Parts Discussed in Thread: OPA2320 , DAC5311 , THS4551 , TVS3301 , TVS2201 , TVS2701 , INA851 , TVS2700 Hi,
We are looking to create a new design to interface industry standard IEPE sensor. We have taken reference from TIDA-010249…
Part Number: TVS2701 Other Parts Discussed in Thread: TVS2201 , STRIKE Hi Team,
we are currently using the following scheme for reverse polarity where TVS is after RPP.
The input is 24VDC from standard industrial supply.
But now we want to ESD protect…
Below are the latest recommendations of devices for multiple interfaces that provide you IEC protection and paired with low capacitance that minimizes impact to bandwidth in the system. Please also refer to our System-Level ESD Guide for more details…
Other Parts Discussed in Thread: ULN2003B , TVS0500 , TVS2200 Hi,
Good Day. I would like to confirm if the devices below can support 230V AC line surge protection for PWM Power Supply Unit.
https://www.ti.com/product/TVS1801
https://www.ti.com/product/T…
Hi,
It seems like the TVS2201 has 4 different protection channels, but the TVS2201 is a single channel device. All 4 IN pins need to be connected to the signal/power rail to provide the protection described in the datasheet. Below is an example of the…
Other Parts Discussed in Thread: ESD122 , TVS2201 , TVS2200 Hi Sir,
My customer need VBUS short protection function in super speed signal trace. TPDXS300 series can't protect SS signal. Is there any solution to protect SS trace on type-c application?…
Part Number: TVS2700 Other Parts Discussed in Thread: TVS2701 , TVS2201 Hello,
I would like to use the flat clamp devices with a +48VDC supply. Can I stack two of the TVS2701 (Vrwm would then be 54V) in series as with stand TVS devices? I realize the dynamic…