Part Number: TVS3300 Other Parts Discussed in Thread: TSM36A Hello,
I would like to protect a power line from overvoltage events. Maximum expected voltage on the line is 33.6 V. Firstly I'm thinking about using SMAJ33A diode, which has Vwrm of 33 V, minimum…
Part Number: TVS3300 Hi Experts
Can someone provide an unencrypted spice model for TVS3300?
You can email me at jim.brinkhurst@ti.com .
The customer is Northrop Grumman Space, and we do have a current NDA with them.
Best regards,
Jim B
Hi Sebastian,
Thank you very much for your reply and I'm sorry to be late my response. They don't have the waveform but they told me the pulse width is less than 10us. Also the EMF sometimes reach to 70~80V.
Q1. Can TVS3300 handle the pulse width…
Part Number: TVS3300 Hi all,
I would like to know about the configuration of TVS3300.
According to the Figure12 (4-20mA current loop) in the application notes of TVS3300, Schottky diode (D0) is located.
TVS3300 Bidirectional Characterization
If I would…
Part Number: TVS3300 Issue: A device (5 Watts) has a regulator that has an absolute max of 40 V.
Possible solution: Use a Flat Clamp TVS diode TVS3300 to shunt current to the ground.
Power Source: PLIU
Nominal voltage = 30 V
Over voltage can result…
Part Number: TVS3300 Other Parts Discussed in Thread: TVS3301 , TVS2700 , , TSM36A Hiya,
Could anyone please suggest me a direct alternative for TVS3300DRVR?
33V flat-clamp surge protection device, WSON (DRV) -6 package.
https://www.ti.com/product/TVS3300…
Part Number: TVS3300 Hi,
This post is regarding SLVAE37 app note, which references TVS3300.
Towards the bottom of page 6, it mentions RDYN of SMAJ33A to be 884mOhm and RDYN of SMBJ33A to be 0.504Ohms. I looked in the datasheets for these parts and did not…
Part Number: TVS3300 Hello,
I'm thinking of use two TVS3300 in a parallel to achieve a higher current capability. I know that is very hard to achieve a true current sharing because of even a little breakdown voltage difference between two diodes. Additionaly…
Part Number: TVS3300 Other Parts Discussed in Thread: LMR36506 , , TVS2700 , INA229 , ATL431LI
I have an application where I have a working voltage of 3V to 60V (up to 65V preferred) and a max clamping voltage of 70V. It will be used to protect the input…