Part Number: TXB-EVM Hello,
I am looking for TXB-EVM board dimensions and any 3D CAD files associated.
Any help is greatly appreciated.
Thank you,
Brooks D'Antonio
Part Number: TXB-EVM Hi Experts, Our customer have a question regarding product: TXB-EVM. There appear to be mounting holes on this board, could you please provide the dimensions? Kind regards, Gerald
Hey Diara,
Adding onto Clemens’ response, further testing with the TXB-EVM can be used to meet your system requirements: https://www.ti.com/tool/TXB-EVM
Regards,
Jack
Hello Koyo,
There seems to be an error with the TXB EVM schematic in which VCCB and Input A are switched.
If you look at the Board Layout for both TXS and TXU EVMs, VCCB (Pin 6) has a bypass capacitor. Apologies for the confusion.
Regards,
Josh
Part Number: AFE7950EVM Other Parts Discussed in Thread: AFE7950 , Hello, team
Can I use the AFE7950 alone without the FPGA board?
I connected the EVM board with usb interface under latte,after bring up, and run mode5,the current of the EVM is about…
Part Number: LSF0204 Hi expert,
Customer want to use LSF0204 for SPI 1.8V <> 3.3V. (I know we have TXU/TXB but let's focus on LSF0204 first cause the design was fixed)
They use 14-24-NL-LOGIC-EVM and mount LSF0204RGYR sample on it.
They are not…
Hello
Please note that the TSW14J56 EVM is now obsoleted. You will now be able to use the TSW14J58 EVM as FPGA based EVM. To do so, please do the following:
1. install HSDC PRO software:
https://www.ti.com/tool/download/DATACONVERTERPRO-SW
2. For all setups…
Hi Camilo,
Today, I test as follow:
1. I connect external 100 MHz clock to J14 on the EVM for LMK_CLK_IN.
2. Execute the High Speed Data Converter Pro
3. Execute the Latte.
4. Set the data rate to 250MHz on the DAC tap of the High Speed Data Converter…
Hi Maynard,
SW1 is hardware reset signal for AFE. SW2 is reset signal for on-board CPLD. Pressing SW1 and SW2 before running the configuration script should not affect functionality of the EVM. The errors seen by the customer are not expected due to that…